EPD Extension Kit for MSP430 LaunchPad
 All Classes Files Functions Variables Typedefs Enumerations Enumerator Macros Pages
Public Attributes | List of all members
ASCII_info_t Struct Reference

The structure of ASCII input information. More...

#include <Mem_Flash.h>

Public Attributes

uint16_t x
 
uint16_t y
 
uint8_t str [16]
 

Detailed Description

The structure of ASCII input information.

Member Data Documentation

uint8_t ASCII_info_t::str[16]

Input string

uint16_t ASCII_info_t::x

x coordinate

uint16_t ASCII_info_t::y

y coordinate


The documentation for this struct was generated from the following file: